• FC BUS OFFLINE - 3rd Party Controllers

    Dear Friends,   When a FC BUS goes offline several times, what is the correct approach for troubleshooting & restoring the bus.   I do understand that faults, baud rates, noise, wiring, or even third p...
    jgutierrez
    last modified by jgutierrez
  • Having issues with pct 10.1 in custom application, palette disappears the very second you go to use. Trying to write a simple exhaust fan control using space humidity for the trigger.

    Any help would be greatly appreciated
    bgibbs
    last modified by bgibbs
  • Introduction

    Hello, my name is Dominic.  I'm a programmer who has been in the field of HVAC controls for a little more than 12 years.  As this field continues to change and grow, it has become very evident that we have t...
    dtturner
    created by dtturner
  • The update is cancelled since all communication failed. - tried Host Name (NAE00108D04B558) but received this error: No such host is known.  (Is the Host Name spelled correctly?)"

    The update is cancelled since all communication failed. - tried Host Name (NAE00108D04B558) but received this error: No such host is known.  (Is the Host Name spelled correctly?)" Is it possible to downgrade fro...
    ly-9100
    last modified by ly-9100
  • Hi,I got good Knowledge in Commercial refrigeration and Transport refrigeration.I would like to attend a crash course in Industrial refrigeration.Pls suggest a suitable course.

    Hi,Kindly advice a crash course in Industrial refrigeration.
  • PCT Problem Starting

    My PCT was running on XP, then windows did an update, now it will not start, when I click on the desktop icon it looks like its going to start then in just rolls back to just the icon and there is no error codes. Any ...
    jefftik
    last modified by jefftik
  • Getting Alert message when commissioning FEC 2610 Controller

    I am trying to load my program in CCT to my field controller and an Alert message shows up stating Diagram could not be loaded. INVALID_VERSION - caf version date = 2015..., controller version date = 2011...   H...
    ninja88880
    last modified by ninja88880
  • Introduce Yourself

    Introduce yourself to the community by telling everyone a little about yourself in this discussion thread. Please say hello, tell us a little bit about what you're currently working on right now and don't forget to in...
    communitymgr
    last modified by communitymgr
  • Why wont NAE upgrade tool run after installing NAE 55 image files?

    I have uninstalled and re installed Upgrade tool, but ever since I installed the image files, it wont wont run.
    ptenwest
    last modified by ptenwest
  • DVN 5000 Forgot Password

    Hello partners,   Actually I have a DVN 5000, and its running, but the DVN have the camera configuration of the latest user, now I want to apply my new parameters but it have some user accounts, and I don't have...
    capg1984
    last modified by capg1984
  • Who can import the NAE*.xml files to a NAE point schedule.xls?

    Hello, I have a customer who wants to create a spread sheet from their existing database of an ADS and 8 NAE's. I know that the NAE*.xml files exported from SCT can be imported to the NAE Point Schedule.xls. Where ca...
    baileth
    created by baileth
  • Graphics Generation Tool question concerning Room Control Modules.

    I`m trying to generate a Room Control Module (multiple rooms) in the GGT tool so that when I click on a room status all relevant setpoints for that room show in the Control Module. I`ve linked the temperature to the r...
    Luktvasslimo
    last modified by Luktvasslimo
  • Help Negative sup temps intermitant (-425.9F), (-312.3F),

    Dear Sir/Madam; After a project was completed some month ago I have noticed after the download I received the following unreliable alarms.   Sup and Ret Temps in (-425.9F, (-312.3F).     My concern ...
    HVAC88
    last modified by HVAC88
  • CCT Custom Applications

    score30
    Open for Voting
    6 votes
    A place to discuss custom programing in CCT and make your controller do more for you.
    bbolton
    last modified by bbolton
  • DVN 5000 password Lost

    hello , i forgot my admin password of our dvn 5000 i read on the manual the procedure to reset but i cant login to the ftp site because the user and pass of the ftp written on manual are not good. Someone can help m...
    stecov
    created by stecov
  • Metasys 6.5 patch install

    Trying to install patch for Metasys 6.5 security vunerability getting   -2147467259 [DBNETLIB][ConnectionOpen (Connect()).]SQL Server does not exist or access denied.
    kraziee
    created by kraziee
  • Honeywell 20K - NTC Scaler

    Converts Honeywell 20K C7041 series temperature sensors for use in PCT. Input should be set as "resistive" . Min Value -50 ohms, Max Value 600,000 ohms, Input Range Low 0 ohms, Input Range High 600,000, Output Range L...
    peterdraper
    last modified by peterdraper
  • 6.5 SCT Passwords

    Dear Friends,     After installing the 6.5 SCT software; is there a defualt password for basic & standard access?   This is a new installation on a standalone laptop.     Thanks,  ...
    jgutierrez
    created by jgutierrez
  • 6.5 SCT Error - Installation

    Dear Friends,   Does anybody understand what this error means?   C:\inetpub\wwwroot\MetasysIII\Tool\Web.config.temp   4-16-2015 14:59:11:1829704 ERROR - there was a problem updating the File C:\in...
    jgutierrez
    last modified by jgutierrez
  • Control Metasys Alarming - Selected Sites

    Friends,   I have just created a new user profile and added only the device objects needed for this user. The user does not have the entire campus, but continues to get all the alarms   How do I eliminate...
    jgutierrez
    last modified by jgutierrez